Part Number: SN65LVDT125A
Hi,
I am looking to create an LVDS multiplexer to switch 6 devices under test (8 pairs each) to 1 acquisition card. 7 pairs are outputs from the DUT, 1 pair in an input to the DUT.
The signalling rate is <75Mbps. The data is not necessarily DC balanced and may contain log chains of identical bits.
My plan so far is to use one and a half SN65LVDT125A for each pair (4+2, allowing for 6 DUTs), cascaded in to another layer of SN65LVDT125A to select between them.
[Extract showing only 2 pairs from the 6 DUTs]
Is this the most appropriate solution from your product portfolio? I can only find larger switches/muxes which do not directly support LVDS and would require layers of translation.
Would cascading to a second layer of switching be required as shown, or could the outputs of the first layer be connected together in parallel instead?
Would termination resistors be required on the unused outputs, as it looks like they would always need to remain internally connected to one of the inputs by selection logic?
This would need 16 IC’s, is there an alternative that uses I2C/SPI etc for the selection control pins, otherwise this could need a lot of IO?
Thank you for the support.