Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK1501: TLK1501- VOD(pp_p) min/max value for AC coupling

Part Number: TLK1501

Hi all,

TLK1501 does not work with the value of 200 ohm in a 50 environment. (when AC coupled mode is chosen.)

We think RREF is directly related to VOD(pp_p). What is the recommend value of VOD(pp_p) for AC coupled mode? Please share min/max value as well.

P.s: If we use 50 ohm instead of 200 ohm, no error is occured.

Regards,