Part Number: TCAN1462-Q1
Other Parts Discussed in Thread: TCAN1042H-Q1, TCAN1472H-Q1
Hi,Ti
Our application environment consists of multiple devices operating under the same 48 V power system, interconnected via a CAN bus.
The devices include motors, cameras, and displays, and the target data rate is 8 Mbps.
Would TCAN1462-Q1 be the recommended choice for this application?
The bus fault voltage rating of TCAN1462-Q1 is ±58 V.
Is this rating sufficient for our application environment?
Under what application conditions would you recommend using an isolated (ISO) CAN transceiver instead?
In the TCAN1462-Q1 user guide, the recommended termination for CAN SIC is not a standard 120ohm resistor, but a termination network that includes a 60ohm filter.
If this termination filter is implemented,
is it compatible with a CAN FD network, especially at high data rates such as 8 Mbps?