Part Number: DP83822IF
Hello TI,
snls505g Fig. 9.2 on p.104 shows the 49R9 resistors connected to "3.3V supply" and the transformer centre taps to AVD Supply. Since AVD could be 1.8V, this connection is unfortunate. Better would probably be to follow TIDA-00928E2(001)_CU and connect the 49R9 resistors to AVD and leave the transformer centre taps only connected to decoupling caps.
Table 8-10 on p. 49 describes possible straps for LED_1 as either Mode 1 or Mode 4. What is the difference between these two, please?
Other strap values seem to be readable in register 0x0467, however, LED_1 is not represented there. Is this correct?