Part Number: DP83822H
Other Parts Discussed in Thread: AM2434, AM6442
Hello,
When performing EtherCAT communication with a configuration in which Port 0 is connected to the EtherCAT MDevice side and Port 1 is connected to an SDevice, I understand that data received from the MDevice (Master) passes through Port 0, goes through the EtherCAT Processing Unit (EPU) inside the PHY, and then reaches the SDevice (Slave) via Port 1.
On the other hand, for transmissions from the SDevice to the MDevice, I understand that the data flows from Port 1 to Port 0 without passing through the EPU.
Is it correct to assume that the DP83822H operates according to this same specification?