Part Number: DP83867E
Hello Experts,
Hello,
A board we are designing has two of these PHYs. One is set up as a RGMII to 1000Base-T transceiver and the other is set up as a SGMII to 1000Base-T transceiver.
On both PHYs, we have added 0 ohm resistors as "Do Not Installs" on the RX_D0, RX_D2, RX_CTRL, LED_1, LED_2, GPIO_0, and GPIO_1 as hooks in the design in case we need to adjust the skew on the RX or TX lines during testing. A few questions...
Question 1: I am a bit confused on the strapping requriements. Per these notes on sheet 40 of the data sheet:
"Note: RX_D1 is not a strap input, but this pin must be populated with the same strap resistors chosen for RX_D0. RX_D0 and RX_D1 form an SGMII differential pair. The dummy straps on RX_D1 are required to provide a balanced load for this SGMII differential pair."
"Note: RX_D3 is not a strap input, but this pin must be populated with the same strap resistors chosen for RX_D2. RX_D2 and RX_D3 form an SGMII differential pair. The dummy straps on RX_D3 are required to provide a balanced load for this SGMII differential pair."
I am assuming this means that we should be putting placeholder 0 ohm resistors on the RX_D1 pin and the RX_D3 pin as well even though they are not strap inputs? Just in case we end up having to put strap resistors on the RX_D0 and RX_D2?
Also, Does this ONLY apply to SGMII or does it apply to RGMII as well?
Question 2: Should we avoid putting any strap resistors on LED_1 and LED_2 if we have them connected to on board LEDs for test?
Question 3: Should we avoid putting any strap resistors on RX_D2/RX_D3 if we are utilizing them as the outputs for SGMII?
Question 4: Per this note in the data sheet "Strap modes 1 and 2 are not applicable for RX_CTRL. The RX_CTRL strap must be configured for strap mode 3 or strap mode 4. If the RX_CTRL pin cannot be strapped to mode 3 or mode 4, bit[7] of Configuration Register 4 (address 0x0031) must be cleared to 0. Autoneg Disable can always be set to 0 when using gigabit Ethernet."
Does this mean that if we do not have any strapping resistors setting the RX_CTRL pin to 3 or 4 we will run into issues? Being that Mode 1 is when the resistors are open.
Regards,
Ross