Part Number: TPS61372
Other Parts Discussed in Thread: TPS61046, TPS61371
Hi,
Does TI have solution can support below feature?
We now found TPS61372, it can support auto mode/force PWM switch when active, but it seems have no output discharge function.
|
Item |
Specification / Requirement |
|
|
Input Voltage |
2.5V ~ 5.5V (Standard Li-Ion range) |
|
|
Output Voltage |
6V and 7V support. |
|
|
Adjustable by HW |
||
|
Output Current |
< 400 mA |
|
|
Operation Mode |
Selectable Mode is Required. (auto/PWM), Need output discharge |
|
|
Package / Size |
Target: As small as possible. |
|
|
Target Reference Dimension: TPS61046 |