Part Number: ESD701-Q1
Hello Team,
We are using the ESD diode ESD701-Q1 in one of our products.
The second pin is connecetd to the Chassis GND.
All ESD diodes are connceted to the chassis GND where it is further connected to the metallic enclosure and then to the protective earth at the 3 pin AC cord.
The signal can swing upto +/-24V.
We have almost 300 ESD diodes in our system.
For some signals we are getting an short between the signal and the chassis GND.
This could because there is an issue in the wiring or could be the ESd diodes are damged.
Is there any way to identify wether the ESD diodes are damged or not.
Looking for your reply