This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD12S016: Power sequencing question (VCCA vs VCC5V)

Guru 14850 points

Part Number: TPD12S016

Hi,

We are using TPD12S016 as an HDMI companion/protection device, and we would like to confirm the power-up / power-down sequencing requirements.

In our system, we have:

  • VCC5V supplied from a 5 V rail (related to the HDMI 5 V line / hot-plug environment)

  • VCCA supplied from the system I/O rail (e.g., 1.8 V / 3.3 V), which may ramp at a different timing than VCC5V

Could you please advise:

  1. Is there any required or recommended sequencing between VCCA and VCC5V (which one must come up first, if any)?

  2. Are there any concerns if VCC5V is present while VCCA = 0 V, or if VCCA is present while VCC5V = 0 V (partial-power condition)?

  3. During these partial-power conditions, do we need any special handling for control pins such as LS_OE and CT_HPD (e.g., keep them low with pull-downs until VCCA is valid) to avoid unintended behavior or back-powering?

Thanks,

Conor