This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS160PT801: DS160PT801 USE?

Part Number: DS160PT801

1. USE  DS160PT801, The following is our application topology. Please help evaluate whether the link risk of redriver placed on Riser2 is controllable.
Topology description: Before the redriver, it passes through a 4-level connector and a 2-level cable. After the redriver, it passes through a 2-level connector and a 1-level cable. The high-temperature loss before Redriver is approximately 23dB, and the high-temperature loss after redriver is approximately 22db.

 

                 S1- Link Risk Assessment -PCIE4.0(SW Managed Link Driver Before)

image.png

 

                    SI- Link Risk Assessment -PCIE4.0(After SW Management Link Driver)

image.png