This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9803: TCA9803 Pull Up Resistance Calculation

Part Number: TCA9803

Hi,

I am using TCA9803 in my PCB for converting 1.8V I2C (at Side A) to 3.3V Level (at Side B)
For the calculation of the pull up resistors at the input of the TCA9803 IC, what should I consider:

VCCA = 1.8V or VCCB = 3.3V should be considered for Rp(min) calculation?
VOL should be 0.4V or some other values?
IOL should be 3mA or 3.3mA?

Kindly suggest me the correct value to be considered?