This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8044A: TUSB8044A in VBUS Source Application

Part Number: TUSB8044A

I am using a TUSB8044A hub in a system that also support 100 W power delivery to the host using the TPS26744E PD Controller. The TUSB8044A hub has the “USB_VBUS” input, which the datasheet says:

“If VBUS needs to be greater (than 11.4 V), then [the] PD controller will need to directly control TUSB8044A USB_VBUS input.”

VBUS on our system will have a maximum voltage of 20 V, so we can’t use the voltage divider approach. What would be the best way to implement this behavior with the TPS26744E?