Other Parts Discussed in Thread: DP83848C
Dear forum,
I want to use a Ethernet PHY DP83848C from National. The PHY should be placed near the CPU on a circuit. This board will be installed at the center of an enclosure. Naturally I'd like to have the RJ45 Ethernet port located on the panel that is 40-50cm far from the circuit.
One solution is to put the CPU, PHY and RJ45 with magnetics on the central board and connect a patch cable (RJ45/RJ45) from the central board to a female/female adapter on the panel.
But I don't have too space on the CPU board and I'd like to don't lose the LED signals for RJ45 connector, so I was thinking if it could be possible to leave CPU and PHY on the central board. I'm going to deliver the MDI signals from PHY to a simple plastic RJ11 6-poles connector (no magnetics) where I can connect the two 10/100 pairs and the two LED signals. With a patch CAT5 cable (RJ11/RJ11), I go on a small board on the panel where I'll have the RJ45 connector with magnetics and LEDs.
What do you think about this approach? How should I care the two MDI signals pairs? Is CAT5 suitable to transport MDI signals from a Ethernet PHY?
Thank you for your answers and suggestions.