Part Number: DS110DF111
Hi,
We are using 2 DS110DF111 retimers(in master mode) connected to single 2Kb external EEPROM . We tried loading EEPROM for configuring retimers as suggested in document:SNLA245.
It was observed that retimer register bytes from 0x57 to 0x5F (Highlighted in yellow in Fig 1) were not provided in the retimer datasheet. But mentioned in SNLA245
Fig 1:

Also the same missing address bytes were called out in the programming guide as highlighted (yellow) in Fig 2 below.
Fig 2:

Also for address byte 0x60 in retimer, it is shown as bits 7:0 are configurable in EEPROM, but only 4 [3:0] bits are able to be set in EEPROM (refer highlighted in blue in Fig 2).
Queries
1. Kindly suggest why such mismatch between the datasheet & programming guide. Which one should be considered?
2. Also confirm if all eeprom configurable bits of DS110DF111 be written in continuous sequence in eeprom? Else suggest the right format.
3. How to configure the bits [7:4] of 0x60 retimer address byte through eeprom configuration?