Part Number: TUSB7340
Hi,
We are using TUSB7340 in our board and connected conected USB2.0 cable on Type A connector.
When we connect the UVC camera which supports USB 2.0 and 1280x 720 resolution in YUYV4:2:2 Format , we are getting 20FPS.
We tried the same experiment with TUSB7340 EVAL kit as well and saw 20FPS only.
Is there any way to increase the BW of TUSB7340 so that we can achieve atleast 24-25FPS for same camera.
Please suggest possible solution for the same,
FYI when we connect it with our laptop with USB2.0 cable we are able to see 25 FPS but with TUSB7340 it is 20FPS only.
is there anything we can try out in driver or some settings to achieve 24-25FPS?
Thanks
Sagar