Other Parts Discussed in Thread: TLK1501
hi..
My Board Structure.
ADC(Video, NTSC)-->FPGA --> TLK1501 -->SFP -------------------------------------- fiber ----------------------------------------- SFP-->TLK1501-->FPGA-->DAC(Video, NTSC)
Process about TLK1501 synchronization and initialization
1. FPGA Configration
2. TLK1501 TxClock 50MHz input(from FPGA), Enable is pull up, Loopen & PRBSEN is pull down.
3. 3 times(Txen = Txer = 0)
4. normal Operation(Txen = 1, Txer = 0)
but almost Link is fail.(somtimes Link is good)
what is the problem?
--------------------------- My source code ----------------------------------
-- Data Transmit --
process(GReset, SerdesClock)
variable CntTx : integer range 0 to 10;
begin
if(GReset = '0') then -- FPGA Reset
CntTx := 0;
OpticSync <= '0';
SerdesTxData(9 downto 0) <= (others => '0'); -- Video
SerdesTxData(12 downto 10) <= (others => '0'); -- Ethernet
SerdesTxData(14 downto 13) <= (others => '0'); -- Audio
SerdesTxData(15) <= '0'; -- Serial
elsif falling_edge(SerdesClock) then
if(OpticSync = '0') then
case CntTx is
-- IDLE State(3 times) --
when 0 => SerdesTxEn <= '0';
SerdesTxEr <= '0';
CntTx := CntTx + 1;
when 1 => SerdesTxEn <= '0';
SerdesTxEr <= '0';
CntTx := CntTx + 1;
when 2 => SerdesTxEn <= '0';
SerdesTxEr <= '0';
OpticSync <= '1';
when others =>
end case;
else -- Normal Operation
CntTx := 0;
SerdesTxData(12 downto 10) <= EthRxDataBuf & EthRxDvBuf;
SerdesTxData(14 downto 13) <= AudioAdcLrck & AudioAdcDout;
SerdesTxData(15) <= VideoADC_Clock1;
if(VideoADC_Clock1 = '1') then
SerdesTxData(9 downto 0) <= VideoInputCh1;
elsif(VideoADC_Clock2 = '1') then
SerdesTxData(9 downto 0) <= VideoInputCh2;
end if;
end if;
end process;