This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1210: Regarding the maximum current flowing through the VBUS terminal

Part Number: TUSB1210

I want to know the maximum current flowing through the VBUS terminal of the TUSB1210.

The electrical characteristics related to VBUS are described in section “6.10 OTG Electrical Characteristics” of the datasheet.

 ●RA_BUS_IN
 ●RB_SRP_DWN
 ●RB_SRP_UP

I suspect that the current consumed at the TUSB1210's VBUS pin is estimated based on one of these resistance values.

6.10's “COMMENTS” section lists 8mA.
Is this understood to be the current consumed by the VBUS terminal?
Also, in that case, is 8mA the maximum value?

Could you please tell me the maximum current consumed by the VBUS terminal?