Part Number: CD74HC4051-Q1
Hi team,
I would like to understand the maximum rating of IO pin input voltage. I don't find a specific withstand voltage for IO pins. Should we refer to the input/output clamp current? If customer can ensure input current can be limited to <20mA, 4051 will not damage even IO voltage up to 7V?
In customer case, they want to know if 4051 IO pins can withstand 7V under 5V VCC condition?
Thanks!
Ethan Wen