This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90LV032AQML-SP: defination of EN and EN_n

Part Number: DS90LV032AQML-SP

As per datasheet page number 2  truth table if EN is low abd EN_n is High IC is desabled and output are tristate, this means when EN is high or EN_n is low other complementry signal is ignored.  the development board sch "www.ti.com/.../snlu195.pdf " Page no 7 , in order to enable the IC J4 and J6 pin 3 and Pin 4 are shoted as per table 1, page 3. 

This means inside the IC EN and Not of EN_N are ANDed and not ORed. Please confirm the same.