This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB211: About the max layout path length of TUSB211

Part Number: TUSB211

Hi Sirs,

I want to know the max layout path length of TUSB211 for layout reference, thanks.

Regards,

Laban LIN

  • Hi Laban,

    For the TUSB211, I would recommend keeping the pre-channel trace length close to ~7 inches if possible.

    Additionally, I would recommend switching to the TUSB211A from the TUSB211. The TUSB211A is a third-generation USB2 redriver that supports both AC and DC boost, as well as RX Sensitivity, while the TUSB211 only supports AC Boost.

    Thanks,

    Ryan

  • Hello,

    Closing thread due to inactivity. If you have any follow-up questions or concerns, feel free to reply.

    Thanks,

    Ryan