I want to use PHY DP83848 from National in RMII mode. Could I connect a pull-up resistor (10k) on MII_MODE pin and leave SNI_MODE floating?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to use PHY DP83848 from National in RMII mode. Could I connect a pull-up resistor (10k) on MII_MODE pin and leave SNI_MODE floating?
Yes. A 10 kOhm pull-up resistor is an appropriate value. All that is required to enable RMII mode is to pull the MII_MODE strap pin (RX_DV) high. The SNI_MODE strap pin (TXD_3) includes an internal pull-down resistor so an external pull-down resistor is not necessary.