This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD6S300A: Unused pins recommendations

Part Number: TPD6S300A
Other Parts Discussed in Thread: PMP40801

Hi, 

I just want to clarify confusion regarding the information given in this topic vs. data seeht. 


Topic: TPD6S300A: What happens if D+ and D- are floating? - Interface forum - Interface - TI E2E support forums 

" What happens if D+ and D- are floating?" -> "You can leave them floating, it should not have an impact on the operation of the TPD6S300A." 

Datasheet: 
"9.2.2.6 How to Connect Unused Pins
If either the RPD_Gx pins or any of the Dx pins are unused in a design, they must be connected to GND". 

In the Reference Desing PMP40801 pins D+ and D- have been left open. 

So, what should we follow? 

Further remarks: 
Datasheet says for pin 16, 17: "Unused pin. Connect to Ground ". However the layout recommendation on Figure 34 doesn't have pins connected to GND. 

BR

Josko
 

  • Hello,

    So, what should we follow? 

    Please follow what is specified in the datasheet.  

    I just want to clarify confusion regarding the information given in this topic vs. data seeht. 

    I believe the topic in the e2e thread is related to a design where the D1 and D2 pins were left floating.  While not recommended per the datasheet, this will not impact the functionality of the clamps nor the ability to provide the Rd resistors in a dead battery situation. 

    It is generally good practice to ground unused pins to prevent a floating node which could raise to a potential that might cause transitions through a transistor threshold, resulting in switching and an increase in power consumption.  My suspicion is that if the D1 and D2 pins are left floating there will be no impact in performance but there may be an increase in the power consumption as specified in the datasheet.

    Further remarks: 
    Datasheet says for pin 16, 17: "Unused pin. Connect to Ground ". However the layout recommendation on Figure 34 doesn't have pins connected to GND. 

    Thank you.  I will submit a request to update the Figure 34.

    Regards,

    Chris

  • Hello Chris,

    thank you for quick response.  

    Regards

    Josko