This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9803: AEC grade drop in alternate for TCA9803DGKR

Part Number: TCA9803
Other Parts Discussed in Thread: TCA9517-Q1

Dear Team,

Can you please suggest AEC grade drop in alternate for TCA9803DGKR?

Thanks in advance!

  • Hi Tanya,

    Our TCA9517-Q1 is AEC-Q100 qualified for auto. 

    It is package drop in, but requires pull-up resistors on both sides of the device unlike TCA9803. 

    Also, the VOLB of TCA9517-Q1 is ~ 0.52 V typical. The offset on B-side is sometimes not compatible with devices whose VIL is < 0.4 V. 

    Regards,

    Tyler