Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
We wish to verify whether there are any issues with the circuit diagram.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Which functional mode are you trying to implement with this design?

Can you also share the connection to the transformer and RJ45 receptacle?
You can also use the attached schematic checklist to check against your design.
Thanks
David
Hi
Connection structure shared.
When setting ETH_RXD3 to “0” in the mode settings, should the R197 resistor be left in the OPEN state? (Is it acceptable not to connect the pull-down resistor?)
We plan to verify the detailed mode settings via the software.
Hi,
It looks like this is a RGMII to Copper Mode design. For RGMII to Copper Mode,
I am also concerned that DP83869 MDI output is connected to the transformer/RJ45 receptacle through a FFC cable. The FFC cable typically is not shielded so the EMI performance is poor, and its crosstalk performance is poor which would affect signal integrity. I would place DP83869, transformer, and RJ45 on the same PCB instead using the FFC cable.
Thanks
David
Hello
I've compiled a pin-specific checklist and am sharing it.
Please review it.
Hi Woohyun,
The schematic checklist and the schematic looks good.
Best,
J