This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1004: TUSB1004 Signal Integrity Simulation - Recommended Similar Model

Part Number: TUSB1004
Other Parts Discussed in Thread: TUSB1002A, TUSB1044, TUSB1146

Hi, 

I understand that TUSB1004 currently does not have IBIS model and I assume similar to answer in this E2E forum thread  there is currently no known timeline for when one will be generated. If not please correct me. 

My question is, can TI recommend an IBIS model for a similar part which may have similar (understanding not exactly the same) behavior as this one, either on the connector side or the host side? Maybe another redriver with same internal host-side receive/transmit buffer?

For example, I see below USB3 redrivers have IBIS models. If planning to use TUSB1004 in design would IBIS models for any of below parts be similar to TUSB1004? Even if the connector side internal driver/receiver are different, do any of below have host side driver/receiver that are same/similar as TUSB1004?

TUSB1002A

TUSB1044

TUSB1146

Thanks!