This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108E-Q1: Required design Clarification for TXS0108E-Q1

Part Number: TXS0108E-Q1
Other Parts Discussed in Thread: TXS0108E

Can i Use TXS0108E-Q1 for the SDIO interface? (Port B is 5V from Host and Port A is 3.3V connected to the host)

 

  • Hi Ramkumar,

    The TXS0108E is compatible with SDIO signaling due to its support for open drain/ push pull drivers and can be used here. Feel free to provide schematic for additional checks. 

    Regards,

    Jack