Team,
1) When using DS38EP100 on a backplane with a max trace length of 12" is there any benefit to using two of these devices - one on Rx side and one on Tx side - on each differential pair of the SGMII (LVDS) interface path?
2) Is there any danger of voltage spiking if either side is hotplugged into the system? If so, is the chip protected against that?
Thanks.