Part Number: TPD1S514
I am specifically looking at the ESD clamping curve information for the protection provided in the TPD1S514x series. I would assume the reverse working voltage is going to be 30V or higher, since the DC input can be up to 30V, but I would like to understand when the TVS starts conducting above 30V, if possible.