This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6746: Termination for DDR2

Part Number: TMS320C6746

Based on the datasheet, it appears that using VTT as specified by JESD79-2 is not recommended.
I am uncertain whether to design the hardware using only series termination without a termination IC.
Your advice would be appreciated.

Figure 6-18. DDR2/mDDR Single-Memory High Level Schematic includes the following note regarding termination settings:

Place termination resistors as needed. Refer to the note regarding termination resistors.

The section regarding termination is:

.4.4.3 DDR2/mDDR
• Parallel termination is not allowed on CLKP/CLKN pins.
• If termination is used, the DDR2/mDDR drive strength should be set to full strength. Otherwise, the
drive strength should be set to half strength.
• No pullups or stubs are allowed on any DDR pins.
• For DQS and D net classes:
– Routes must be point-to-point. – Skew matching across bytes is not needed nor recommended. – Skew between the two classes should not exceed 25 mil.
• Clock and DQS net class trace lengths need to be routed such that the skew between the two net classes meets the tDQSS timing parameter.

6.11.3.9 DDR2/mDDR Signal Termination
No terminations of any kind are required in order to meet signal integrity and overshoot requirements. Serial terminators are permitted, if desired, to reduce EMI risk; however, serial terminations are the only type permitted. 

Please advise how to interpret the above.

  • Hi, you can design the board for series termination, and adjust the resistance as needed.  If you can obtain robust operation with 0ohm resistors, then you have the opportunity to design out the resistors on a future revision of the board.

    Regards,

    James

  • Hello James.

    Does this mean I can design without VTT termination?

    Thank you in advance.
    Yamada

  • Yes, VTT termination for DRAM is needed when a larger number of memory components and longer traces are present.  If you are using a single memory device with C67x, typically you can design without VTT termination.  The best sources for information on point-to-point termination can be found on the Micron website in their technical notes TN-46-06 and TN-46-14.  The C67x was designed to use a series termination as opposed to a pull-up to VTT to minimize the number components needed and to minimize the power.  Using a VTT termination introduces a constant DC current that is always present, this is eliminated in the series termination model.  If the design and routing guidelines presented in the datasheet are followed, acceptable signal integrity will be achieved without a VTT supply.

    Regards,

    James

  • Hi,James


    I reviewed the technical documents you provided.
    I will complete the design based on the recommended layout.

    Thank you very much.
    Yamada