This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI85: EOL

Part Number: SN65DSI85

Hi

Is this chip still EOL? Are there any alternatives? SN65DSI85ZQER

  • Hi Gareth,

    Currently, this device is ACTIVE on TI.com. 

    Best regards,
    Ikram

  • Thank you for your information.

    I have the following question:

    1. What is the difference between SN65DSI85ZXHR and SN65DSI85ZXHR.A?

    2. We need to switch from single DSI to dual LVDS. Is this done by modifying the register settings via I2C?

    Thanks

  • Hi Gareth,

    1. The orderable part number for both are the same on ti.com

    2. The DSI input can either be in single or dual mode, and the LVDS output can also be set to single or dual port. These are set by modifying the register settings via that you can find in the datasheet. We would recommend using the DSI Tuner GUI to enter the settings, display timings for input and output video, and get an output with all the register settings. 

    The datasheet "7.4.1 Operating Modes" section described the register settings for DSI and LVDS.


    Best regards,
    Ikram