Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIOL221: About LDO output (VOUT)?

Part Number: TIOL221

Dear Technical Support Team

When the IO-Link is disconnected (LP-LM open) and the 5V input pin (V5IN) is also open,
is it acceptable to apply 3.3V to the LDO output (VOUT)?
※Please ensure the VSEL pin is floating.

This inquiry is to confirm safety during microcontroller programming
when configuring the system to feed the output from VOUT into the microcontroller.

Best Regards,

ttd

  • Yes, this should be OK because the voltage on the VOUT pin is less than the abs max ratings.  I will also note that the datasheet states that when the V5IN supply is used for the LDO (i.e VSEL pin = Floating), the LDO will be disabled.  However the LP-LM supply would also be required.

    Regards,

    Jonathan

  • Hi Jonathan,

    Thank you for your reply.

    >However the LP-LM supply would also be required.

    In my case , this assumes no power supply to the LP-LM. Is that not possible?

    If not, please advise if there is any workaround using an external circuit or similar.

    Best Regards,

    ttd

  • Hi ttd,

    I'm sorry you didn't understand my response.  My point wast that even if LP-LM was supplied and V5IN was not, the LDO would be disabled.

    I do not see an issue with having 3.3V on the VOUT pin when the LP-LM is not supplied.

    Regards,

    Jonathan