This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83849ID: Request suggestions for 2-Port Ethernet Switch ICs / Dual PHY with single MAC

Part Number: DP83849ID

Hi,

DP83849ID is a dual PHY with 2 dedicated MACs required. Can you suggest some 2-Port Ethernet Switch ICs or Dual PHY with single MAC options available with TI that provides MII/RMII interface?

We are currently evaluating 2-Port Ethernet Switch options and have encountered a limitation in available microcontroller pins.

The DP83849ID, while functionally suitable, requires two dedicated MAC interfaces, which is not feasible in our current design.

Could you please suggest alternative 2-Port Ethernet Switch ICs or Dual PHY solutions that can operate with a single MAC from TI and support MII or RMII interfaces?

We are specifically looking for configurations that help reduce pin count while maintaining reliable dual-port Ethernet functionality. 

Thank You.

Regards,

Bhabana