Part Number: DP83TG720R-Q1
Is Far end loopback is xMII Reverse Loopback With External Data-Gen(as mentioned in Datasheet)?
Also suggest the Ethernet PHY which has 100/1000Base T1 supports SQI, Test Mode 4, Far end loopback.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83TG720R-Q1
Is Far end loopback is xMII Reverse Loopback With External Data-Gen(as mentioned in Datasheet)?
Also suggest the Ethernet PHY which has 100/1000Base T1 supports SQI, Test Mode 4, Far end loopback.
Hi Ganapriya,
Can you please share a block diagram of the far end loopback you are intending to implement?
We do not currently have an Automotive Ethernet PHY that supports both 100 and 1000BASE-T1. Do you need both speeds supported?
Best regards,
Greg