Part Number: TLIN2021A-Q1
Other Parts Discussed in Thread: TLIN4029A-Q1
Hi Team
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLIN2021A-Q1
Other Parts Discussed in Thread: TLIN4029A-Q1
Hi Team
Hi Ramya,
1. There should be no such differences and the abs max ratings specified in the data sheet should be absolute for both. However, VSON packages may often have lower inductance which can help with the layout level ESD performance but not different die level clamp thresholds.
2. 60 V as specified in the data sheet. If damaged, this more than likely implies transients > the applied 54 V and more than the specified 60 V was observed on the IC pin, most likely due to inductance on the bus.
3. Unfortunately, we cannot and recommend utilizing the information specified in the data sheet at all times.
4. Most likely overvoltage above the abs max ratings similar to 2.
5. Unfortunately, the data sheet is strongly recommended as staying within the limits would help in mitigating such damages. May also include series resistors for faults, TVS diodes at the connector, proper grounding etc.
6. Yes, and would also recommend a device with abs max ratings above ISO's 48 V upper limit I.e., see TLIN4029A-Q1 rated up to 70 V, thanks.
Best Regards,
Michael.