This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN2451-Q1: Component Class under ISO26262 part 8 Clause 13

Part Number: TCAN2451-Q1

If we are going to use the component for only the following functions, what would be the evaluation of the Component Class under ISO26262 part 8 Clause 13

  1. Power supply generation and NOT for monitoring
  2. Watchdog(Monitor the Microcontroller)

 

Will that be fit under Class II or Class III?