Part Number: AM26C31
Hi,
So a while back I posted a question regarding your differential line drivers and if it would be possible to achieve a close to rail to rail output voltage when no termination was present on the outputs. Specifically talking about the AM26C31I chip. So you confirmed (Bobby) that this would not be an issue and that we would be able to get close to rail to rail, see my earlier post:
I confirmed this by testing with the AM26C31IN package:

So I confidently paced them into our design but with a different package: AM26C31IPWR . However the output characteristics are completely different. The output voltage with the same load now only reaches ~3.6V...

Which is not sufficient for what we are trying to do. Could you possibly provide support and why this could be? Is it true that the internals of these chips are different between the packages?
See our schematic:

These signals go directly into the UCC21710QDWRQ gate drivers. But around the same output when there is no load attached (so best case scenario).