Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN3413: IBS model fails parser check, Part TCAN3413DR

Part Number: TCAN3413

I just downloaded the IBS file for CAN bus buffer part TCAN3413DR from the TI.com website. It fails the IBS parser check and here is the log:

IBISCHK7 V7.2.0

 

Checking 

NOTE (line  122) - Pulldown Minimum data is non-monotonic

NOTE (line  123) - Pulldown Typical data is non-monotonic

WARNING - Model canH: C_comp should not be specified when C_comp_pullup, C_comp_pulldown, C_comp_power_clamp or C_comp_gnd_clamp is specified

WARNING - Model 'canH': Vmeas timing test load parameter should be specified

NOTE (line  772) - Pulldown Minimum data is non-monotonic

NOTE (line  845) - Pullup Minimum data is non-monotonic

WARNING - Model canL: C_comp should not be specified when C_comp_pullup, C_comp_pulldown, C_comp_power_clamp or C_comp_gnd_clamp is specified

WARNING - Model 'canL': Vmeas timing test load parameter should be specified

NOTE - Combined Pulldown for Model: canL Minimum data is non-monotonic based on piece-wise linear interpolation

NOTE - Combined Pullup for Model: canL Minimum data is non-monotonic based on piece-wise linear interpolation

NOTE - Combined Pulldown for Model: canH Typical data is non-monotonic based on piece-wise linear interpolation

WARNING - Model canH: The [Rising Waveform]

      with [R_fixture]=30 Ohms and [V_fixture]=3.3V

      has TYP column DC endpoints of  2.80V and  3.27v, but

      an equivalent load applied to the model's I-V tables yields

      different voltages ( 2.80V and  3.30V),

      a difference of  0.00% and  5.75%, respectively.

WARNING - Model canH: The [Falling Waveform]

      with [R_fixture]=30 Ohms and [V_fixture]=0V

      has TYP column DC endpoints of  0.38V and  2.70v, but

      an equivalent load applied to the model's I-V tables yields

      different voltages ( 0.38V and  2.75V),

      a difference of  0.05% and  2.23%, respectively.

NOTE - Combined Pulldown for Model: canH Minimum data is non-monotonic based on piece-wise linear interpolation

ERROR - Model canH: The [Falling Waveform]

      with [R_fixture]=30 Ohms and [V_fixture_min]=0V

      has MIN column DC endpoints of  0.12V and  1.93v, but

      an equivalent load applied to the model's I-V tables yields

      different voltages ( 0.11V and  2.15V),

      a difference of  0.17% and 10.87%, respectively.

WARNING - Model canH: The [Rising Waveform]

      with [R_fixture]=30 Ohms and [V_fixture_max]=0V

      has MAX column DC endpoints of  0.95V and  3.27v, but

      an equivalent load applied to the model's I-V tables yields

      different voltages ( 0.95V and  3.22V),

      a difference of  0.06% and  2.16%, respectively.

ERROR -

    Component 'TCAN': Diff_Pin 'CANL' not previously declared in Pin section.

ERROR -

    Component 'TCAN': inv_pin 'CANH' not previously declared in Pin section.

 

Errors  : 3

Warnings: 7

 

File Failed

  • Hi Joseph,

    Today is a holiday. Please give some time for some feedback, thanks.

    Best Regards,

    Michael.

  • Hi Joseph,

    I have followed up with the design team in parallel and waiting their feedback.

    In the meantime, could you help confirm if any concerns with TCAN33X IBIS Model? Thanks.

    Best Regards,

    Michael.

  • Michael. There are multiple failures of the IBS model when using the committee parser and the Hyperlynx parser. These are the errors. Note where it says ERRORS below. 

    IBISCHK7 V7.2.0


    NOTE (line 122) - Pulldown Minimum data is non-monotonic
    NOTE (line 123) - Pulldown Typical data is non-monotonic
    WARNING - Model canH: C_comp should not be specified when C_comp_pullup, C_comp_pulldown, C_comp_power_clamp or C_comp_gnd_clamp is specified
    WARNING - Model 'canH': Vmeas timing test load parameter should be specified
    NOTE (line 772) - Pulldown Minimum data is non-monotonic
    NOTE (line 845) - Pullup Minimum data is non-monotonic
    WARNING - Model canL: C_comp should not be specified when C_comp_pullup, C_comp_pulldown, C_comp_power_clamp or C_comp_gnd_clamp is specified
    WARNING - Model 'canL': Vmeas timing test load parameter should be specified
    NOTE - Combined Pulldown for Model: canL Minimum data is non-monotonic based on piece-wise linear interpolation
    NOTE - Combined Pullup for Model: canL Minimum data is non-monotonic based on piece-wise linear interpolation
    NOTE - Combined Pulldown for Model: canH Typical data is non-monotonic based on piece-wise linear interpolation
    WARNING - Model canH: The [Rising Waveform]
    with [R_fixture]=30 Ohms and [V_fixture]=3.3V
    has TYP column DC endpoints of 2.80V and 3.27v, but
    an equivalent load applied to the model's I-V tables yields
    different voltages ( 2.80V and 3.30V),
    a difference of 0.00% and 5.75%, respectively.
    WARNING - Model canH: The [Falling Waveform]
    with [R_fixture]=30 Ohms and [V_fixture]=0V
    has TYP column DC endpoints of 0.38V and 2.70v, but
    an equivalent load applied to the model's I-V tables yields
    different voltages ( 0.38V and 2.75V),
    a difference of 0.05% and 2.23%, respectively.
    NOTE - Combined Pulldown for Model: canH Minimum data is non-monotonic based on piece-wise linear interpolation
    ERROR - Model canH: The [Falling Waveform]
    with [R_fixture]=30 Ohms and [V_fixture_min]=0V
    has MIN column DC endpoints of 0.12V and 1.93v, but
    an equivalent load applied to the model's I-V tables yields
    different voltages ( 0.11V and 2.15V),
    a difference of 0.17% and 10.87%, respectively.
    WARNING - Model canH: The [Rising Waveform]
    with [R_fixture]=30 Ohms and [V_fixture_max]=0V
    has MAX column DC endpoints of 0.95V and 3.27v, but
    an equivalent load applied to the model's I-V tables yields
    different voltages ( 0.95V and 3.22V),
    a difference of 0.06% and 2.16%, respectively.
    ERROR -
    Component 'TCAN': Diff_Pin 'CANL' not previously declared in Pin section.
    ERROR -
    Component 'TCAN': inv_pin 'CANH' not previously declared in Pin section.

    Errors : 3
    Warnings: 7

    File Failed

  • Hi Joseph,

    Yes, the IBIS model I shared is for a different model. Or are you implying both models give the same errors?

    Best Regards,

    Michael. 

  • Hello:

    There is only one IBS file that I am focusing on, that is TI File "SLLM508.zip" which contains the compressed IBS file "tcan34xx.ibs". This is the only file I'm interested in, and the only file I've written about in this case. Perhaps you are referring to the IBS checker report, which I repeated, since I was not sure we are fully communicating. I submitted this case one week ago, have you heard from those responsible, as to whether they also get IBS parser checking errors, or are working to fix this?

  • Hi Joseph,

    I have followed up internally to resolve your "tcan34xx.ibs" concerns.

    However, I would recommended to use this different TCAN33X IBIS Model for now until the 34x model is resolved, thanks.

    Best Regards,

    Michael.

  • Hi Joseph,

    Please see below for the updated design IBIS model, thanks.

    tcan34xx.ibs

    Best Regards,

    Michael.

  • I agree the new file is much better, and produces no errors from the parsers. I still receive warnings, though but likely they are not as serious as the original errors. I will proceed to use the new tcan34xx.ibs file for my simulations of the CAN bus. TY. "Resolved."