Part Number: TCAN4550
Hi,
I think there is a small discrepancy in the TCAN4550 datasheet, regarding the INH output state?
Text says: The INH function is on in all modes but sleep mode.
State diagram agrees with Text: INH is only off/floating in Sleep mode (e.g. is On=H in UVIO mode)
But Mode Overview table says: INH is Off in both Sleep and UVIO Protected mode.
Which is correct? Is the INH state a safe HW indicator for "TCAN4550 is definately in Sleep mode of all the modes"?
And another question for the State Diagram:
States Standby Mode, TSD Protected and UVIO Protected show "Wake Sources: WAKE" or "CAN, WAKE" inside the state block. I can see the wake event effect when in Sleep mode. But what is the effect of a wake event (bus or pin) in the other states mentioned above?
Thanks