Part Number: DP83826AE
Hi team,
I am using an XMC4800 to interface DP83826AE PHY for ECAT communication. I have the following signals coming from the XMC4800 ESC(ethercat slave controller) to PHY.
- TXD[0:3], TXEN and TXCLK
- RXD[0:3], RXERR, RXDV and RXCLK
The above signals are coming for both the PHY's individually and the common signals for the two PHY's are:
- MCLK, MDIO
- 25MHz clock IN to XI pin on PHY from ESC clockout pin
Can you please provide the design guidelines as follows:
- Can you please provide the length matching and impedance matching details for each signal where applicable.
- What are the length matching groups we need to make in these signals ?
- If applicable, what are the group-to-group length matching constraints?
- What are the constraints or rules for routing the 25MHz clock from XMC to PHY?
Thank You
Sanath