This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4020BI: TUSB4020BI Malfunction

Part Number: TUSB4020BI

Hi Team,

We are using TUSB4020 in our design

We have connected FT4232 and CY7C68013A from the HUB. Suddenly we see below issue in few of our boards. Powers and clocks are ok 

I see the GRSTn is sometimes going high even before stable 3.3V few boards. But, I do not see any issue in connecting USB on those boards

Could you provide us some inputs regarding below issue

Screenshot 2026-02-19 171228.png

Awaiting for your respose

 

 

Thanks,

Rohini

 

  • HI Rohini:

       Can you send schematic for review first?

    Best

    Brian

  • Hi Brain,

    Please find the sch below

    Thanks,

    Rohini

  • Hi Rohini:

       I didn't find any issue in schematic.

        Did FT4232 and CY7C68013A connected to hub downstream ports? Do they need VBus to start working?

       Can you take waveform for  1.1V , 3.3v and GRSTz  signal?

    Best

    Brian

       

  • Hi Brain,

    Yes, FT4232 and CY7C68013A are connected to HUB downstream ports. Those devices are self powered. Taking powers from Board rails and don't need VBUS

    PFA- 1.1V,3.3V and GRSTz Power up sequence

    Note:

    1. on some board we see GRSTz is going high even before 3.3V is not in stable state . but we do not see any issue with that boards

    When we tried increase the capacitance value to 2.2uF on GRSTz Pin, we didn't see any change in the HUB behavior

    2. Previously we had mostly only CY7C68013A  on the downstream path and kept FT4232  on reset in most of our boards

    Now we have enabled both FT4232 and CY7C68013A(both are out off reset) in our latest design. We started seeing this issue on this revision boards

    Thanks,

    Rohini

  • Hi Rohini:

       Power on sequence looks ok from your waveform .

       What is fail rate from tested board? Can you send downstream port schematic as well?

    Regards

    Brian