This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: SFD function

Part Number: DP83822I

I have a question about the SFD feature.
In section 8.3.3 of the datasheet, the SFD functions are: LED_0, LED_1 (GPIO1), COL (GPIO2), RX_D3 (GPIO3) Int/PWDN_N and CRS pins.
In the datasheet discribed,
' The IEEE 1588 PTP pin Select Register (PTPPSEL, address 0x003E) is able to route both transmit and receive indications to LED_0 (GPIO1), COL (GPIO2), CRS and INT/PWDN_N, '
Pins and markings.

 

Is LED_0 (GPIO1) a typo for LED_1 (GPIO1)?
If it's not typo, LED_0, CRS pin is set from register 0x003E. Is it correct to recognize that when assigning to GPIO pins, it is set by registers 0x0462, 0x0463?