Part Number: TCAN1462-Q1
Hello TI experts,
I am considering using the TCAN1462-Q1 CAN-FD transceiver in a design where the CAN-FD data phase needs to run at 8 Mbps. In the datasheet overview, the part is described as supporting “Classical CAN and CAN FD up to 8 Mbps,” but the detail is limited.
Specifically, I am looking for solid technical evidence and clarification on the following points:
-
Is the 8 Mbps data phase rate supported as a guaranteed, validated capability of the transceiver?
-
Is this part tested and characterized for 8 Mbps across temperature, voltage, and process variation ?
-
Or is the 8 Mbps figure only a nominal maximum rating under ideal conditions?
-
-
Does the transceiver fully support 8 Mbps within the ISO 11898-2/CiA 601-4 physical layer specifications?
-
The datasheet mentions compliance with ISO 11898-2:2016 and CiA 601-4 but does not explicitly show timing, slew, or electrical parameters at 8 Mbps.
-
-
Are there example test results, validation plots, or application notes demonstrating error rates or signal integrity performance at 8 Mbps?
-
Are there any recommended network constraints required to achieve reliable 8 Mbps operation?
-
Cable length, node count, termination, stub length, or signal improvement recommendations.
-
It would be very helpful if someone could point me to specific datasheet sections, app notes, or validation documentation that confirm whether 8 Mbps is practical and robust for this part in real network conditions, as opposed to just being listed as a “max” signaling rate.
Thanks in advance!
Best Regards,
Manoj.