Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869, DP83869EVM
Hi,
We are using the DP83869HM Ethernet PHY in SGMII mode (1000 Mbps) with a 2-supply configuration. The SGMII interface is connected to the MPU, and the MDI signals are connected to an RJ-45 connector.
Kindly review the attached schematic diagram and clarify the following questions:

- Is it require to connect 3.3 V supply, whenever the voltage level of IO pins is 1.8V?
- Are the EMI filters used on the 1.8 V, 2.5 V, and 1.1 V supply rails sufficient for noise suppression?
- Are the pull-up resistors connected to RX_D[3..0], JTAG_TMS, JTAG_TDI, and JTAG_CLK correctly configured to set SGMII to Copper mode?
- We are using the PHY with VDDIO = 1.8 V. Are the current connections correct for this configuration?
- The clock frequency for SGMII mode is 625 MHz. What should be the crystal oscillator frequency used for SGMII operation?
- Is a 3-supply configuration required, or is a 2-supply configuration sufficient? If a 3-supply configuration is required, under what conditions would it be necessary?
- Why and when are coupling capacitors required between the MPU and the Ethernet PHY on the SGMII lines?
Thank You
Rajeev Kumar