Part Number: TCAN4550
Hello,
are the GPO2_CONFIG, GPIO1_CONFIG and GPIO1_GPO_CONFIG settings in the Modes of Operation and Pin Configuration Register (h0800) still relevant when the TCAN4550 is used in Test Mode with TEST_MODE_CONFIG = 1?
E.g. GPIO1 is the RXD input (from the external CAN transceiver) in this mode. Must GPIO1_CONFIG be set to "10 = GPI – Automatically becomes a WD input trigger pin." or could it be left "00 = GPO"?
Thanks