Part Number: DS125DF1610
Hi Experts,
I am writing to seek advice regarding CDR locking issues we are experiencing on our load board.
We are following the same procedure that was successful on the EVM:
1. Set RX input to 550 MHz.
2. Configure VCO to 10.8 GHz with a /4 divider to target a 2.7 GHz PRBS7 signal.
3. Perform CDR reset for each channel.
While this works consistently on the EVM, the results on our load board are inconsistent: specifically, while some channels are stable, others fail to achieve CDR lock or experience frequent unlocks
.Are there any retimer registers or CTLE/DFE settings you suggest we adjust to compensate for potential board-level or channel-to-channel variations?
Any suggestion is will be appreciated.