This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB9261DEMO: Maximum data conversion speed

Part Number: TUSB9261DEMO
Other Parts Discussed in Thread: TUSB9261

Hi,

I recently ran a simple test on my PC with your TUSB9261DEMO connected to a SDD, with SSD capable of writing in 520 MB/s.

While i ran a cmd prompt on my PC to test the speed through TUSB9261 the prompt said "Disc Sequential 64 Write 151.20 MB/s".

How fast can TUSB9261 convert USB data into SATA?

Best regards,

Andreas

  • Also, is there a way to increase the conversion speed?

  • Hi Andreas,

    Is this being used with a USB2 or USB3 application? I.E is the USB cable being used a USB3 cable.

    Is this being done with a SATA drive or an SSD? Typically, SATA tends to have lower speeds.

    While i ran a cmd prompt on my PC to test the speed through TUSB9261 the prompt said "Disc Sequential 64 Write 151.20 MB/s".

    Is this test the PC writing to the SSD through the TUSB9261DEMO?

    As far as I am aware, there is no way to control/increase the speed of the TUSB9261 aside from the cable being used and the SATA drive generation.

    Also, is this data in Mb or MB? If MBps, that's more data than Mbps.

    Thanks,

    Ryan

  • Hello,

    Closing thread due to inactivity. If you have any follow-up questions or concerns, feel free to reply.

    Thanks,

    Ryan