Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS31-32EVM: Is it usable with SPI hall effect position sensor

Part Number: SN65LVDS31-32EVM
Other Parts Discussed in Thread: SN65LVDS31-33EVM

Hello,

I have a hall effect position sensor with SPI output (Micronas HAL3900).

Does the SN65LVDS31-32EVM can be used to pass SPI through cables from this sensor to master µc ?

Communication clock frequency is about 1MHz.

In this case, is 1 board enough ?

Best Regards,

Mathieu LALLEMANT