This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TG721S-Q1: DP83TG721S-Q1 - Schematic Review

Part Number: DP83TG721S-Q1

Hi TI Team,
Please find the schematic of Ethernet DP83TG721S-Q1 for review, Kindly share your valuable feedback on the same.

The design Considerations are,

  1. Interface: SGMII
  2. Application: 1000BASE-T1 to Automotive Connector
  3. Clock Source: 25 MHz Crystal (CL = 8 pF) [is there any Specific formula for CL to be used in schematics considering the stray capacitance]
  4. TC10 enabled configuration.
  5. Need wake up function enabled

image.png