This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD11-HT: Fab Information on two parts and Latch up testing

Part Number: SN65HVD11-HT
Other Parts Discussed in Thread: TRS3122E,

Can you tell me if the SN65HVD11-HT is manufactured on the same fab line as the TRS3122E?  They are both listed as being Power BiCMOS and I need to know if they are from the same fab?  Are these parts tested in accordance with JESD78 for Latch up and if so what is the passing level for the device? Thanks, Brian