This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN4550: TCAN4550 AP under WIN10 or WIN11

Part Number: TCAN4550
Other Parts Discussed in Thread: BOOSTXL-CANFD-LIN

Hi sir, 

Do we have TCAN4550 AP under WIN10 or WIN11?

Customer wants to test. 

Thanks a lot!

  • Hi Sean,

    No, the TCAN4550 has a SPI interface that is generally connected to a microcontroller or embedded processor.  Many embedded processors run a Linux OS and there is a tcan4x5x driver embedded into the Linux Kernel that will communicate with the TCAN4550.  But I am not aware of any embedded processors running Windows that will directly communicate through SPI at the hardware level, and there is not a driver available.

    With Windows you will generally need some sort of SPI controller module that has a software API, or a microcontroller or processor that has a USB interface and has been programmed to configure and communicate with the TCAN4550 through SPi.

    Please refer to the following resources:

    TCAN45xx Software User's Guide (Link)

    MCAN User's Manual (Link)

    BOOSTXL-CANFD-LIN (LInk)

    Regards,

    Jonathan